Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20763
  • Release Date : 2018/08/21 16:10
  • Update : 2018/09/04 15:06
  • Print

About changing the direction of the cable entrance for the terminal box

Answer

Please refer to the section "Terminal box installation location and direction of lead wire outlet" of the general catalogue.
However, GM-J2 series is not supported.
In addition, we can not correspond indoor type (GM-S, GM-SSY, GM-SHY, range from 0.1kW to 0.4kW) using resin terminal box.
Product Name
Geared Motors
Series
Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries