Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20802
  • Release Date : 2018/08/22 16:24
  • Print

FR-XC

What are the restrictions for performing the harmonics suppression?
Category : 

Answer

- Both 200 V and 400 V can be used only with the capacity 22 kW or higher.
- The rated current (capacity) is derated. (For the detail, refer to the Instruction Manual.)
- The dedicated box-type reactor (FR-XCB) is required.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries