FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-XC
FAQ
FR-XC
What are the restrictions for performing the harmonics suppression?
- Category :
Answer
- Both 200 V and 400 V can be used only with the capacity 22 kW or higher.
- The rated current (capacity) is derated. (For the detail, refer to the Instruction Manual.)
- The dedicated box-type reactor (FR-XCB) is required.
- The rated current (capacity) is derated. (For the detail, refer to the Instruction Manual.)
- The dedicated box-type reactor (FR-XCB) is required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option