Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20804
  • Release Date : 2018/08/22 16:24
  • Print

FR-HAL/FR-HEL selection

When using the vector motor, should I select the FR-HAL/FR-HEL of the one-rank higher capacity for the vector motor?
Category : 

Answer

Not required. Select it according to the capacity of the vector motor used.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?