FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800/FR-F800
FAQ
FR-A800/FR-F800
The P3 terminal is added depending on the capacity. Is it possible to connect the brake unit or brake resistor with both P/+ and P3?
- Category :
Answer
When connecting to the P/+, the current flows in the inrush circuit at the regenerative driving. This regenerative current may generate losses in the inrush circuit, which causes the overheat and damage of the inverter. Thus, connect the brake unit or brake resistor to the P3 terminal when the P3 terminal is prepared.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800