Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20824
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800 "Parameter for the communication setting"

Pr.1300 to 1400 are described as "Parameter for the communication setting". For what communication are these parameters used?
Category : 

Answer

These parameters are used for the communication compatible with the communication protocol of the Ethernet IP of the HMS optional circuit board (A8NEIP_2P).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries