Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20861
  • Release Date : 2018/08/22 16:24
  • Print

Operation mode switch of the FR-A800/F800

Pr.79 is set to "0", however, the external operation is not switched to the PU operation with the PU/EXT button. What can be its cause?
Category : 

Answer

When Pr.551 is set to "3" (Command right to the USB connector at the PU operation), or when the USB is connected, the operation is not switched.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries