Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20876
  • Release Date : 2018/08/22 16:24
  • Print

FR-A8TR

As the restriction of the FR-A8TR, it is described that the terminals +24, 10E, 4, and STOP are unavailable when the FR-A8NC is used. What is the reason for that?
Category : 

Answer

Because when the FR-A8NC and FR-A8TR are used together, the wiring to the terminals becomes physically difficult.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries