Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20897
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800

When tuning the SF-V5RU by Pr.71 = 33, does the tuning result change between Pr.9 = 0 and Pr.9 = Rated motor current setting?
Category : 

Answer

Yes. When Pr.9 = 0, turning is performed with the inverter rated current.
Always set the rated motor current.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries