FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > Terminal response time
FAQ
Terminal response time
What is the terminal response time of the FR-A800? Can I adjust the terminal response time so that it becomes equal between before and after the replacement from the A700 series?
- Category :
Answer
It is 2 to 3 ms. By setting Pr.289 Inverter output terminal filter and Pr.699 Input terminal filter, the FR-A700 can be compatible with the response of the terminals of the FR-A700. Adjust it according to the system with a guide of 5 to 8 ms.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800