Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20917
  • Release Date : 2018/08/22 16:25
  • Print

FR-A8NC/FR-A8AX

Can I set the frequency from the CC-Link and FR-A8AX?
Category : 

Answer

The frequency setting in the communication cannot be used together with FR-A8AX. The priority of the FR-A8AX is equal to the second terminal analog input and it is enabled in the following operation mode. External operation mode, External/PU combined operation mode 2 (Pr.79 = 4), NET operation mode (Pr.339 = 1)
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries