Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20924
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-R2R

How is the initial roll calculated?
Category : 

Answer

The calculation is performed by two modes. One method calculates the current winding diameter automatically by moving the dancer roll from lower limit position to the target position at start. The other method calculates the current winding diameter from the line speed and actual rotation speed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800 Plus

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries