Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20926
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-R2R

Are there any devices other than the inverter required for the tension control dedicated to winding/unwinding?
Category : 

Answer

A tension sensor such as a dancer roll is required for speed control. Because an actual line speed input is required for the winding diameter calculation by the actual line speed method, devices such as a speed detection device is required.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800 Plus

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries