Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20943
  • Release Date : 2018/08/22 16:25
  • Print

CC-Link

Is it possible to import all signals of warning and alarm via the CC-Link using FR-A800+FR-A8NC?
Category : 

Answer

For output signals, up to 10 points (RXn2 to RXB) can be assigned. It is possible if the number of the importing signal points are within this range.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries