Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20977
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

Though the control circuit temperature can be monitored with Pr.52=98, is any alarm generated when the control circuit temperature rises?
Category : 

Answer

No alarm occurs due to the abnormal temperature. In the main circuit, alarms such as heatsink overheat will be occurred.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries