Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21014
  • Release Date : 2018/08/22 16:25
  • Print

Parameter copy to the USB memory

Can I write the USB memory parameter copy file (*.cp1) to the inverter when the model is different (such as when replacing the FR-A800 with FR-F800)?
Category : 

Answer

No. Writing is not available when the model is different. Writing the parameter copy file using a USB memory device is available only for the same models. Otherwise, the error "rE4" is displayed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries