Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21016
  • Release Date : 2018/08/22 16:25
  • Print

Gain adjustment under the speed control

What happens with the response when Pr.820 is set to 0%?
Category : 

Answer

Since the lower limit has been internally set, 3% or less is recognized as 3%.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries