Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21048
  • Release Date : 2018/08/22 16:25
  • Print

PLC function

When changing the value of SD1144 (Set frequency writing (RAM)) with Y24 (Set frequency writing command (RAM)) ON to change the frequency using the PLC function, why does the frequency not change?
Category : 

Answer

The setting is enabled at the Y24 start-up. The frequency cannot be changed when Y24 is always ON. Turn ON Y24 when writing a frequency.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries