Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21050
  • Release Date : 2018/08/22 16:25
  • Print

RS-485 and analog input

When applying the frequency command with the FR-D700, is there any difference between the RS-485 and analog input?
Category : 

Answer

The time from when the frequency command is applied until it is reflected on the operation of the motor is different. For the analog input, the multiple analog input terminals such as second terminal and fourth terminal are switched and read sequentially. Therefore, the response of the RS-485 is improved compared to the analog input.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-D700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries