Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21061
  • Release Date : 2018/08/22 16:25
  • Print

PM motor control

For the FR-F700P, the control method is IPM motor drive and for the FR-F800, it is PM motor drive. Are there any differences?
Category : 

Answer

For the FR-F700P, only dedicated IPM motor (MM-EFS, MM-THE4) can be driven. For the FR-F800, the name is different because PM motors manufactured by other companies can be driven by performing offline auto tuning.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries