Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21070
  • Release Date : 2018/08/22 16:25
  • Print

The number of input terminals

Is the number of input terminals the same as that of the F700P series?
(For F700P: STF, STR, STOP, RH, RM, RL, JOG, RT, MRS, RES, AU, CS)
Category : 

Answer

The number of terminals: There are the same input terminals as F700P and the following terminals (4 points) are added. Safety: SI1, SI2, SIC 24 V power supply: + 24 *The terminals SI1, SI2, and SIC are dedicated to the safety. Functions cannot be changed as other terminals.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries