Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21110
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

Is the installation compatible with the A500(L) series? FR-A520(L)-0.4K to 90K, FR-A540(L)-0.4K to 280K, FR-A540L-375K and 450K
Category : 

Answer

- The installation size is compatible for the following capacities.
Compatible: 200 V class 90K or lower, 400 V class 7.5K or lower and 18.5K to 280K- The installation size is compatible for the following capacities by using the optional intercompatib
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries