Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21119
  • Release Date : 2018/08/22 16:26
  • Print

Parameter unit

Can the parameter unit (FR-PU07(BB)) used?
Category : 

Answer

The FR-PU07(BB) can be used with some restrictions.* The major restrictions are as follows.
- Pr.1000 or later cannot be set.
- Alarms or warnings that are added to the A800/F800 series cannot be displayed.
- The parameter copy function is not available.
- The troubleshooting cannot be displayed properly.
- Operation to USB memory devices is unavailable.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries