FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Parameter unit
FAQ
Parameter unit
Can the parameter unit (FR-PU07(BB)) used?
- Category :
Answer
The FR-PU07(BB) can be used with some restrictions.* The major restrictions are as follows.
- Pr.1000 or later cannot be set.
- Alarms or warnings that are added to the A800/F800 series cannot be displayed.
- The parameter copy function is not available.
- The troubleshooting cannot be displayed properly.
- Operation to USB memory devices is unavailable.
- Pr.1000 or later cannot be set.
- Alarms or warnings that are added to the A800/F800 series cannot be displayed.
- The parameter copy function is not available.
- The troubleshooting cannot be displayed properly.
- Operation to USB memory devices is unavailable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800