Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21134
  • Release Date : 2018/08/22 16:26
  • Print

FR Configurator

When the parameter data of the FR-A700 is read with FR-SW3, why Pr.551 is set to "65535"?
Category : 

Answer

This is because the version of the FR-SW3 is old, and the version of INV is new (Pr.551 = 9999 is added for the products manufactured in December 2011 or later). In the previous version of the FR-SW3, Pr.551 = 9999 cannot be recognized, and displays 65535 (FFFF). Update the FR-SW3 to the latest version.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries