Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21161
  • Release Date : 2018/08/22 16:26
  • Print

Setting resolution switching

The display does not change even Pr.811 (Set resolution switchover) is set to "1". Are there any other parameters to be set?
Category : 

Answer

Check the setting value of Pr.37 (Speed display). When the machine speed is set, Pr.811 is disabled. Change the setting to the rotation speed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries