Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21162
  • Release Date : 2018/08/22 16:26
  • Print

Orientation control

After the X22 signal is turned ON, the motor keeps rotating at the speed of the setting value of Pr.351 (Orientation speed). What is the possible cause?
Category : 

Answer

The following reasons are possible.
- The signal of Z phase does not exist. (It is not returned normally.)
- The setting of Pr.359 encoder rotation direction is reversed.
- The setting of Pr.369 number of encoder pulses is not correct.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries