FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Rotation speed display
FAQ
Rotation speed display
When the Pr.37 (Speed display) or Pr.144 (Speed setting switchover) is set to change the display to the machine speed or rotation speed, is the display of frequency data saved in the faults history switched to the machine speed or rotation speed?
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
It is not switched. The frequency at the fault saved in the faults history is always displayed in frequency [Hz].
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700