FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Stop selection
FAQ
Stop selection
By setting Pr.250 (Stop selection) to 0 during JOG operation, can the output be shut off when the start command is turned OFF?
- Category :
Answer
No. During JOG operation, deceleration stop is performed even though Pr.250 is set.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700