Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21247
  • Release Date : 2018/08/22 16:26
  • Print

Replacement

When the FR-A500 is replaced with FR-A700, which parameter number of the FR-A700 corresponds to Pr.903 (Frequency setting voltage gain) of FR-A500?
Category : 

Answer

It is Pr.125 (Terminal 2 frequency setting gain frequency). Adjust the slope with C4 (903) (Terminal 2 frequency setting gain) as necessary.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries