FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Operation method
FAQ
Operation method
I want to input start command from an external source to the terminal STF and operate the frequency command by rotating the setting dial as the potentiometer. How should I configure the setting?
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
Set Pr.79 (Operation mode) to "3" and Pr.161 (Frequency setting/key lock operation selection) to "1".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700