Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21256
  • Release Date : 2018/08/22 16:26
  • Print

CC-Link communication

I want to switch the operation mode to NET operation mode to start the inverter and set the frequency in the CC-Link communication, but it does not switch. How should I set the parameters? And I want the operation mode to be fixed to NET operation mode.
Category : 

Answer

After setting Pr.79 (Operation mode selection) to "2" and Pr.340 (Communication startup mode selection) to "10", reset the inverter (or power ON again) to start and fix the mode to NET operation mode.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries