Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21262
  • Release Date : 2018/08/22 16:26
  • Print

Parameter read

Pr.77 (Write selection) cannot be read with the parameter unit (FR-PU07). What should I do?For what are they used?
Category : 

Answer

By setting Pr.160 (User group read selection ("Extended function display selection" for D700)) to "0", all the parameters can be read.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries