Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21267
  • Release Date : 2018/08/22 16:26
  • Print

Frequency setting signal

While the current 4 to 20 mA is input to terminal 4, the FWD blinks and operation does not start. Pr.267 (Terminal 4 input selection) is set to "0" and voltage/current input selection switch of terminal 4 is turned ON ("I" for E700 and D700). What are the possible causes for this?
Category : 

Answer

Check the AU signal (AU - SD). To use the terminal 4, the AU signal (AU - SD) needs to be turned ON. Turning ON the AU signal (AU - SD) disables the terminal 2.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries