Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21271
  • Release Date : 2018/08/22 16:26
  • Print

Motor coasting

Answer

To set the motor to coasting state, the following methods are available: 1. Set Pr.250 (Stop selection) to "0" and turn OFF the start command.
2. Short the terminals MRS and SD.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries