FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Brake resistor
FAQ
Brake resistor
How much is the regenerative brake duty when the built-in brake resistor is used in the FR-A700?
- Category :
Answer
When the built-in brake resistor is used, the regenerative brake duty is as follows:200 V 0.4K to 3.7K: 3%, 5.5K to 7.5K: 2%400 V 0.4K to 7.5K: 2 %
The capacity other than the above does not have a built-in brake resistor.
The capacity other than the above does not have a built-in brake resistor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700