Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21282
  • Release Date : 2018/08/22 16:26
  • Print

Specifications

The specification of the inverter is three-phase 200 V power input. Can I drive the three-phase 200 V motor by inputting single-phase 200 V?
Category : 

Answer

It can be driven by connecting single-phase 200 V to the terminals R and S.
In this case, the load current must be one-third or less of the inverter rated current.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries