Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21294
  • Release Date : 2018/08/22 16:26
  • Print

Auto tuning

Even though auto tuning is performed, the monitor indicator remains as "1" and RUN LED blinks. What are the possible causes?
Category : 

Answer

With the monitor indicator "1", there is no problem with the parameter setting of auto tuning.
Check if the terminals MRS and SD are not shortened in the wiring of the inverter.
(Check if the signal to externally stop the operation is not input.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries