FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-PA07
FAQ
FR-PA07
When using the option FR-PA07 and external terminals, how do I switch the setting dial and multi-speed selection?
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
Since the multi-speed is given a higher priority, the setting by the setting dial is not enabled unless all of the multi-speed signals are OFF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700