FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Graph function in FR-Configurator
FAQ
Graph function in FR-Configurator
The current, frequency, and load factor are selected as display items of the graph function in FR Configurator (FR-SW3-SETUP-WJ).
Even though the time setting of the horizontal axis is changed from "1500 ms/Div" to "700 ms/Div" and "Enter" is clicked, the setting is not changed.
The version of FR Configurator is "2.00", the OS of the personal computer is WindowsXP, and FR Configurator is connected to the personal computer with the USB.
Even though the time setting of the horizontal axis is changed from "1500 ms/Div" to "700 ms/Div" and "Enter" is clicked, the setting is not changed.
The version of FR Configurator is "2.00", the OS of the personal computer is WindowsXP, and FR Configurator is connected to the personal computer with the USB.
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
Even the USB is used, FR Configurator requires at least 50 ms sampling time (for each monitoring item).
In this case, since three types of data are monitored, it takes at least 150 ms.
When creating a graph, since 10 pieces of data are input in 1 Div, 150 ms × 10 = 1500 ms is necessary to create 1 Div for three types of data.
The time shorter than above cannot be set.
To decrease the setting time, decrease the items to be monitored.
In this case, since three types of data are monitored, it takes at least 150 ms.
When creating a graph, since 10 pieces of data are input in 1 Div, 150 ms × 10 = 1500 ms is necessary to create 1 Div for three types of data.
The time shorter than above cannot be set.
To decrease the setting time, decrease the items to be monitored.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700