FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Connection cable of FR-Configurator
FAQ
Connection cable of FR-Configurator
I want to communicate with FR-Configurator (FR-SW3-SETUP-WJ) using the USB connector.
Is the Mini-B indicates the standardized Mini-B connector?
Is the Mini-B indicates the standardized Mini-B connector?
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
It is the standardized Mini-B connector.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700