Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21323
  • Release Date : 2018/08/22 16:27
  • Print

Terminal indicator lamp

I want to check the operation at the motor position because the conveyor is long. Can I install the indicator lamp between terminals U and V to receive the light with phototube and check the operation?
Category : 

Answer

The inverter outputs the peak voltage 300 to 400 VDC of the bus voltage not in a pure sine wave but a in a PWM waveform.
Check if the lamp to be connected can withstand the above voltage.
When the inverter frequency is low, the low voltage prevents the lamp from being lit (Reconsider the use of the lamp.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries