FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Brake resistor
FAQ
Brake resistor
Is the brake resistor MYS120W40 (inverter option) shared when the inverter capacity of 2.2K and 3.7K are used?
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
It will be the shared type.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700