FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameter display setting
FAQ
Parameter display setting
When Pr.80 (Motor capacity) and Pr.81 (Number of motor poles) are set, "Er4" is displayed and the settings are disabled.
How can I set them?
How can I set them?
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
Normally, Pr.80 and Pr.81 are the parameters that can be changed when the operation is stopped in the PU operation mode.
The "Er4" is a mode designation error. Check the operation mode.
When Pr.79 is set to "2", the parameter setting cannot be changed since External operation mode is activated.
The "Er4" is a mode designation error. Check the operation mode.
When Pr.79 is set to "2", the parameter setting cannot be changed since External operation mode is activated.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700