FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Input phase loss
FAQ
Input phase loss
An error "E.ILF" is displayed with the FR-E700.
Since it was an input phase loss error, I checked the power supply but the phase was not lost.
Are there any other possible causes?
Since it was an input phase loss error, I checked the power supply but the phase was not lost.
Are there any other possible causes?
- Category :
Answer
The FR-E700, D700, F700PJ may activate input phase loss protection "E.ILF" if the phase-to-phase voltage of the power supply has become largely unbalanced.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ