FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Applied terminal
FAQ
Applied terminal
When connecting a potentiometer with the terminals 10, 2, and 5 of the inverter, do I have to use the shielded cable?
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
As described in the instruction manual, use the shielded cable or twisted cable to avoid the influence of noises.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700