Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21358
  • Release Date : 2018/08/22 16:27
  • Print

UL standard

The UL standard of the United States asks the current (kA) of SSCA (short circuit current ratings).

How much is it?
Category : 

Answer

Both 200 V class and 400 V class are suitable for use in a circuit capable of delivering not more than 100 kA rms symmetrical amperes, 264 V maximum (528 V for 400 V class).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries