FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > UL standard
FAQ
UL standard
The UL standard of the United States asks the current (kA) of SSCA (short circuit current ratings).
How much is it?
How much is it?
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
Both 200 V class and 400 V class are suitable for use in a circuit capable of delivering not more than 100 kA rms symmetrical amperes, 264 V maximum (528 V for 400 V class).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700