Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21359
  • Release Date : 2018/08/22 16:27
  • Print

PU operation

1. Can I input the emergency stop during the PU operation?  

2. Can I reverse the input of the emergency stop?  

3. Will the operation continue when the operation is stopped by turning ON the emergency stop, and then turned OFF the emergency stop again?
Category : 

Answer

1. Yes.

2. Set Pr.17 to "2".  

3. If the start signal is ON, the operation continues even the emergency stop is OFF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries