FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > MRS setting
FAQ
MRS setting
1. What is the difference between MRS and Pr.250 = "0"?
2. Do I have to set both of them?
2. Do I have to set both of them?
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
1. For MRS, coasting starts when the MRS contact turns ON. For Pr.250 = "0",IM is coasting immediately when the start signal is turned OFF.
2. No. Set either one.
2. No. Set either one.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700